Module 1 - Describing Functions
 
  Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self Test
 
 Lesson 1.1: Describing Functions Symbolically
 

In this lesson you will define a function symbolically in the Y= editor and investigate the function on the Home screen.


Defining a Function

The function you will define is f(x) = 2x2 - 5x - 3.

  • Press , the first graphing key, to open the Y= editor.
  • Deleting Functions in the Y= Editor

    You can clear lines in the Y= editor by moving the cursor to the desired line with the up or down arrow keys, or , and then pressing .



  • Enter the function f(x) = 2x2 - 5x - 3 in Y1 by pressing .

Evaluating a Function

Now that you have successfully defined the function f(x) = 2x2 - 5x - 3 in Y1, you can evaluate the function at x = 2 by evaluating the expression Y1(2) on the Home screen.

  • Return to and clear the Home screen by pressing [QUIT] .
  • Open the Variables menu by pressing and then select the Y-Variables submenu by pressing .
  • Select the Function submenu by pressing .
  • Paste the variable Y1 to the Home screen by pressing .
  • Finish the expression by pressing .
  • Evaluate the expression by pressing .

Editing the Last Entry

If you want to evaluate the function at x = 3 next, you can recall and edit the last expression on the Home screen rather than entering in the entire expression.

  • Press [Entry] to recall the last expression.
  • Move the cursor to the 2 by pressing twice.
  • Overwrite the 2 with a 3 by pressing .
  • Display the result by pressing .

Finding Zeros of Functions

One of the
A zero of a function is a value of the independent variable that makes the function zero. In other words, solutions to f(x) = 0 are the zeros of the function f.
zeros of the function f(x) = 2x2 – 5x - 3 is x = 3 because f(3) = 0, as shown in the screen above. This function has another zero.

1.1.1 Evaluate the function at other values of x until you find the other zero. When you have found the other zero, click here for the answer.

Guess and Check

When you tried several values until you found the second zero, you used a method called

The Guess and Check method can be used to find zeros (or roots)of a function. Use the "Guess and Check" method to find the zeros of a function as follows:

First guess a value for the independent variable and evaluate the function there.

If the value of the function is not zero, pick another value of the independent variable and evaluate the function again. Considering the results from previous guesses might improve your later guesses

Continue in this manner until a zero is found.

Guess and Check.

The Relationship Between Zeros and Factors

Many polynomial expressions, like 2x2 - 5x - 3, can be factored and there is a relationship between the zeros and the factors of the function.

1.1.2 Find the zeros of f(x) = 2x2 - 5x - 3 by factoring. Compare the zeros of the factors to the zeros of the function f(x) = 2x2 - 5x - 3 found earlier. Click here for the answer.

For polynomial functions. x = r is a zero of f if and only if x - r is a factor of f(x).


< Back | Next>
  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy