Exam Acceptance – Work It
Permitted for testing
The calculators listed in the chart below are permitted for testing and accepted on several college entrance and Advanced Placement* exams.
Test | TI-Nspire Handhelds with Clickpad and TI-84 PLUS Keypad |
TI-Nspire CAS Handheld with Clickpad |
TI-Nspire Handhelds with Touchpad and TI-84 PLUS Keypad |
TI-Nspire CAS Handheld with Touchpad |
---|---|---|---|---|
SAT | • | • | • | • |
ACT | • | • | ||
PSAT/NMSQT* | • | • | • | • |
AP* | • | • | • | • |
Praxis™† | • | • | • | • |
IB™ | • | • |
State assessments
The TI-Nspire handheld is permitted on a growing number of state assessments including those in Arkansas, Colorado, Connecticut, Illinois, Indiana, Kansas, Kentucky, Louisiana, Maine, Maryland, Massachusetts, Michigan, Minnesota, Missouri, Montana, New Hampshire, New Jersey, New Mexico, New York, North Carolina, North Dakota, Oregon, Pennsylvania, Rhode Island, South Carolina, South Dakota, Tennessee, Texas, Utah, Vermont, Virginia, Washington, West Virginia, Wisconsin, and Wyoming.
Other states including Delaware and Mississippi permit TI-Nspire in TI-84 mode. To find out if your state permits TI-Nspire technology, go to the state information map or contact your state's education department.
Test preparation
The Press-to-Test feature for TI-Nspire and TI-Nspire CAS handhelds is a fast way to configure student handhelds on exam days. Using a special key sequence on TI-Nspire and TI-Nspire CAS handhelds, the built-in Press-to-Test feature temporarily blocks access to certain features not allowed during testing. The temporarily disabled features can be easily restored after the exam for continued use during classroom lessons and activities.
The Press-to-Test feature also works with the TI-Nspire handheld's interchangeable TI-84 Plus Keypad.
Download the latest TI-Nspire operating system that includes the new Press-to-Test feature.
For instructions on using the Press-to-Test feature, go to Press-to-Test.
To learn more about other testing resources, request the TI Test Prep Solutions Kit.
Please check with your school district or state department of education to determine whether Press-to-Test is approved for exams.
*SAT and AP are registered trademarks of the College Entrance Examination Board. PSAT/NMSQT is a registered trademark of the College Entrance Examination Board and National Merit Scholarship Corporation. ACT is a registered trademark of ACT, Inc. None of these were involved in the production of nor do they endorse this product. Policies subject to change. Visit www.collegeboard.com and www.act.org.
**The TI-84 Plus Keypad is not included or compatible with the TI-Nspire CAS handheld and may not be included with TI-Nspire handheld when sold outside of North America.
Praxis and IB are trademarks of their respective owners
†A graphing calculator (including the TI-Nspire and TI-Nspire CAS) is allowed for the following Praxis tests:
0065 Mathematics: Pedagogy
0069 Middle School Mathematics
A graphing calculator (including the TI-Nspire and TI-Nspire CAS) is required for the following Praxis tests:
0061 Mathematics: Content Knowledge
0063 Mathematics: Proofs, Models, and Problems, Part 1
No other Praxis mathematics test allows a graphing calculator.