Site: US and Canada

Algebra Using the TI-83 Plus / TI-84 Plus Online Course

Course Outline and Take this Course

How to take this course
We've made it easy! No log-in, no time limit, just click on the module in which you are interested below and get started today.

Course Outline
Introduction
Get acquainted with how to take this course including tips on navigation.

Module 0: Getting Aquainted
This module will examine the following:
• three different zones of the TI-84 plus and what each zone does
• how to reset defaults and examining what happens to different features when this is done
• how to enter arithmetic expressions with addition and implied multiplication (parenthesis)
• how to evaluate exponential expressions with repeated multiplication, exponential function key and the pretty print (or preset) exponents

Module 1: Building the Bridge From Arithmetic to Algebra
This module will examine the following:
• solving algebraic expressions and examining patterning by entering values in alphanumeric values and using the last answer function.
• converting fractions to lowest terms.
• entering and graphing functions using the y= editor
• resizing windows manually to create friendly viewing windows and using the trace feature to solve for missing values in a function
• setting up tables and scrolling through tables to find missing data values

Module 2: Number Patterns and Sequences
This module will examine the following:
• creating a recursive sequence on the home screen
• storing multiple answers in the calculator and using the answer feature to create a table/list containing a recursive sequence on the home screen
• using the seq command to generate lists of data in the list editor and creating scatter plots.
• graphing equations to represent data in a scatter plot and using the trace/ table features to solve values

Module 3: Using Lists to Build Algebraic Thinking
This module will examine the following:
• learning an algorithm to multiply by 11
• entering data values in lists and enter formulas in the list editor
• using the set up editor to display lists and rearranging lists in the list editor
• using the catalogue to locate commands and using the sum command to add elements in a list
• using the y = editor and tables to input independent values to obtain dependent values for a function

Module 4: Draw on Your Knowledge of Coordinates
This module will examine the following:
• using graph window presets such as zstandard, zdecimal, zinterger, to create friendly viewing windows
• manually changing the window settings to create friendly viewing graph windows and manually setting the center of a window
• graphing lines squares, circles using tools from the draw menu and clearing drawings
• drawing on the graph screen using the draw tools from the home screen and storing/recalling drawings
• downloading and using TI Connect to capture drawings on the home screen

Module 5: Transformations
This module will examine the following:
• use the set up editor and the alpha lock feature to name and create lists
• using graph window presets such as zoomstat and zsquare to create friendly viewing windows and manually changing window settings
• performing operations on lists to reflect, translate and dilate graphs
• using the augment and dim commands to change the size of lists

Module 6: Operations in Algebra: Rational Numbers and Expressions
This module will examine the following:
• comparing and ordering rational numbers using relational operators and using the sort command for lists
• add, subtract, multiply, and divide rational numbers
• convert decimals to fractions
• using the last answer feature
• store numbers in alphanumeric variables and solving for expressions, using relational operators to compare algebraic expressions
• entering and comparing algebraic expressions and using graphs/ tables to compare expressions

Module 7: Proportional Reasoning
This module will examine the following:
• using the y = editor to graph functions and to solve ratios using the trace, value and intersection features
• using the answer feature to convert decimal values for time to minutes, seconds
• looking for patterns by performing operations on lists, storing values, graphing linear functions and scatter plots
• using the Calc menu and the value command to solve for missing values

Module 8: Solving Equations
This module will examine the following:
• using the guess-and-test method to solve equations
• entering expressions and using concatenation on home screen to solve expressions
• entering functions using the y = editor and using the table feature to find missing values
• Solving Equations Algebraically store values and compare answers with expressions with rational numbers
• using y= editor to graphing and using the Calc menu to find intersection points
• expressing answers in fractional form


Module 9: Solving Linear Inequalities
This module will examine the following:
• solving inequalities in one variable using concatenation and relational operators
• solving inequalities using tables and graphs by entering equations into y = editor and using tables/ graphs to solve for missing values
• using relational operators to graph linear inequalities by using the y = editor to enter equations and inequalities
• using graphs to examine inequalities and determine intersection points

Module 10: Percent Applications
This module will examine the following:
• determine discounts by entering expressions and inequalities on home screen using relational operators
• determining sales tax and tips through solving inequalities with tables, graphing and home screen
• solving inflation and depreciation problems using graphs and the Calc menu.

Module 11: Solving Problems Involving Linear Functions
This module will examine the following:
• using the list editor and attaching formulas to a list to create dependent values form independent values
• entering functions and using tables to accept independent values into table and solve for dependent values
• perform operations on functions, find intersection points and use tables to find missing values

Module 12: Equation of a Line
This module will examine the following:
• comparing the slopes of lines using the y= editor and graphs
• graphing lines in slope-intercept form and finding intersection points
• create scatter plots and graph functions to draw lines to fit data points

Module 13: Programming and Lines
This module will examine the following:
• how to write a program to find slope and y- intercept
• using the random integer feature to create an equation for a line in slope intercept form - -load a program using TI Connect


Module 14: Linear Data Collection Activities
This module will examine the following:
• examining Hooke’s Law
• using the seq feature to generate data and storing values into variables
• graphing functions and using tables to input independent variables in table
• finding points of intersection using the Calc menu

Module 15: Linear Data Collection Activities with the CBR
This module will examine the following:
• loading of data using TI Connect
• using the y = editor to graph functions
• store values using alphanumeric variables

Module 16: Relations and Functions
This module will examine the following:
• drawing and labelling points
• drawing horizontal and vertical lines and drawing the inverse of a function,
• drawing a circle using the home screen
• entering functions into the y = editor and using the table feature to enter independent values
• entering data values into lists
• using change in lists to find the common difference, slope

Module 17: Systems of Linear Equations
This module will examine the following:
• using home screen to guess and check solutions and to find the intersection point of two functions
• graphing functions and performing mathematical operations on functions in the y= editor
• entering matrices and finding a solution using the rref (row reduced echelon form) feature

Module 18: Compound Inequalities and Systems of Inequalities
This module will examine the following:
• entering functions into the y = editor and finding points of intersection
• using Boolean and relational operators to graph the solution of an inequality
• graphing an inequality and using the home screen to test values

Module 19: Factoring Trinomials
This module will examine the following:
• checking linear factors using relational operators and the home screen
• storing values into alphanumeric variables,
• entering and comparing functions with relational operators and graphs
• using the Calc menu and the zero feature to solve trinomials for x=0 to compare factors

Module 20: Transformations of Quadratic Functions
This module will examine the following:
• graphing multiple functions from one function,
• using zoom decimal window to determine information from graphs
• using list editor to enter and generate data values
• graphing data using scatter plots
• using the Calc menu to find the maximum point and vertex
• enter functions into the y = editor and using the home screen to verify solutions

Module 21: Solving Quadratic Equations
This module will examine the following:
• entering functions to find the maximum point or vertex and checking answers on the home screen
• entering functions and finding the point of intersection and using tables to verify answers
• entering expressions on the home screen
• using alphanumeric variables to store numbers and entering expressions on the home screen
• enter the functions and use the zero feature to determine solutions
• running a program called quadfrom

Module 22: Exponential Functions
This module will examine the following:
• entering expressions on the home screen and using exponent key,
• converting decimal numbers to simplest form fractions
• using the last answer feature to generate a table of values on the home screen,
• using repeated multiplication, exponential function key and the pretty print or preset exponents
• entering functions and use the table to solve expressions
• entering functions and find intersection point

Module 23: Exponential, Rational, and Radical Functions
This module will examine the following:
• using recursion on the home screen
• entering functions using the y = editor and comparing tables or graphs,
• finding the intersection point

Module 24: Absolute-Value Equations and Inequalities
This module will examine the following:
• enter functions and finding the point of intersection
• using relational operators with tables and drawing graphs
• using zoom feature (zoom in) to see points of intersection
• using one function to draw multiple functions and storing values in alphanumeric variables

Module 25: Using Lists and Graphs
This module will examine the following:
• inserting, deleting, overwriting values in a list
• creating a scatter plot
• drawing vertical and horizontal lines to examine the vertical line test

Module 26: Linear Regression
This module will examine the following:
• entering data into lists to create scatter plots and tracing values
• entering functions to compare lines of best fit, use linreg feature to determine slope and y-intercept,
• using the Catalogue menu to turn diagonistics on/off to see correlation coefficients

Module 27: More Linear Regressions
This module will examine the following:
• comparing lists to find first level differences in a list
• perform stat calculations (mean) on a list,
• storing values in alphanumeric variables
• entering functions in y= editor and using linreg feature to determine slope and y-intercept


Version: 1.20130516.105409 rev. 47177 (Production)