Site: US and Canada

TI-36X Pro Scientific Calculator

Advanced, four-line scientific calculator, with higher-level math and science functionality, is ideal for computer science and engineering courses in which graphing technology may not be permitted.

36xpro

Key features

  • Four-line display
  • One- and two-variable statistics
  • MultiView™ display shows multiple calculations at the same time on screen
  • Select degrees/radians, floating/fix, number format modes
  • Choose from three solvers: numeric equation, polynomial and system of linear equations
  • Display a defined function in a tabular form
  • Determine the numeric derivative and integral for real functions
  • Perform vectors and matrices using a vector and matrix entry window
Exam acceptance

The TI-36X Pro scientific calculator is approved for use on SAT*, ACT*, and AP* exams.

*SAT, ACT & AP are registered trademarks of the College Board, which was not involved in the production of and does not endorse this product. Policies subject to change. Visit www.collegeboard.com.

Ideal for

● Algebra 1 and 2     ● Geometry         ● Trigonometry       ● Statistics
● Calculus                 ● Biology             ● Chemistry            ● Physics
● Computer Science  ● College math   ● College Science    ● College Engineering

TI36Pro-View-multiple-calculations

View multiple calculations at the same time

Compare results and explore patterns on-screen with the MultiView™ display, which supports up to four lines.

TI36Pro-see-math-exactly

See math exactly as it appears in textbooks

See math expressions, symbols and stacked fractions exactly the way they appear in textbooks — no need to adapt to a technical syntax; also provides quick access to frequently used functions.

TI36Probuilt-in-solutions

Built-in solvers

Intuitive prompts allow one to easily solve numeric equation, polynomial and system of linear equations.

TI36xProbuilt-easy-to-use-mode

Easy-to-use mode menu

The menu is structured for easy, intuitive access to commands; select degrees/radians, floating/fix, Classic/MathPrint™ or number format.

TI36Pro-explore-table-of-values

Explore (x,y) table of values

Students can easily explore an (x,y) table of values for a given function, automatically or by entering specific x values.