Site: US and Canada

TI-Nspire™ CAS with Clickpad

CAS Comparison Chart

CAS stands for Computer Algebra System. Using a CAS system on a calculator means that the calculator will be able to perform symbolic manipulation of variables without a value being assigned to those variables. The comparison chart below gives some examples of how answers might look different on TI-Nspire CAS as opposed to TI-Nspire and also some of the additional functionality of TI-Nspire CAS. Here are some of examples of the types.


Step-by-step calculations
TI-Nspire handheld
     TI-Nspire CAS handheld

Error displays without a defined variable to continue the problem

 

Show each problem-solving step without making arithmetric errors


Arithmetic calculations

TI-Nspire handheld
     TI-Nspire CAS handheld

Simplified expressions are approximated in decimal form

Mathematical constants (Π, e) and variables (x, y) provide approximate numeric answers

 

Simplified expressions keep their mathematical structure

Mathematical constants and variables are recognized and simplified symbolically

Simplify trigonometric identities

Will give exact values for special angles on the unit circle


Algebraic calculations

TI-Nspire handheld
     TI-Nspire CAS handheld

Find approximate values for solution of an equation

 

Exact and approximate values for solutions of an equation

Polymonials are factored and expanded

Complex solutions and zeros can be found


Calculus calculations

TI-Nspire handheld
     TI-Nspire CAS handheld

Find numerical approximations of the derivative at a point

Find numerical approximations of the integral value for a given interval

 

Calculate limits of an expression (including right-hand and left-hand limits)

Find derivatives of function as well as find a derivative at a point

Find values for definite and indefinite integrals

Uses correct notion for derivatives and integrals as students would see in a textbook or write on paper



CAS can help students develop algebraic patterns. In these examples, CAS is used as a learning tool and can help students discover the algebra themselves. This allows for a solid conceptual understanding and can provide a basis for learning of by-hand symbolic manipulation.

Nspire Cas Screen

  Nspire Cas screen


Version: 1.20130516.105409 rev. 47177 (Production)