Site: US and Canada

Algebra 2 : Binomial Probabilities

Published on March 30, 2012

Overview

Students simulate rolling a die and keeping track of the numbers of successes and failures by using the randBin command.

Key Steps

  • Image

    In Problem 1, students can either use the Roll Dice simulation of the Prob Sim app or roll a real die to investigate binomial probabilities.

    Each student rolls the die five times and records the result where a 6 is a success. They are to repeat this experiment nine more times. They track their results in a table provided on their worksheets.

  • Image

    In a second table, they record the number and percentage of successes in each of the 10 experiments. The number of successes should sum to 10 and the percent of successes (in decimal form) should sum up to 1, this will represent the experimental binomial probabilities.

  • Image

    Students will use the randBin command that simulates binomial experiments. This will help students see how the simulated results compare to their actual results.

Version: 1.20130516.105409 rev. 47177 (Production)