Solution 37799: What TI-Innovator Hub Apps are available for the TI-84 Plus CE graphing Calculator?
What TI-Innovator Hub Apps are available for the TI-84 Plus CE graphing Calculator?
Frequently Asked Questions about the TI-Innovator™ Hub App for the TI-84 Plus CE.
What is the TI-Innovator™ Hub App?
The TI-Innovator™ Hub App adds the HUB menu to the programming menu on a TI-84 Plus CE graphing calculator.
This menu option makes it easy to select commands that are commonly used when creating programs to use with the TI-Innovator™ Hub.
How do I know whether I have the TI-Innovator™ Hub App?
To determine if the Hub app is loaded on your TI-84 Plus CE calculator, follow these steps:
1) Press 2nd [mem]
2) Select option “2: Mem Management/Delete…”
3) Select option “A: Apps”
The TI-Innovator™ Hub App is listed as “Hub” in the list of apps.
Confirm that the Hub is listed.
What version of the TI-Innovator™ Hub App do I need?
Version 5.2 of the TI-Innovator™ Hub App is the latest version and runs on the TI-84 Plus CE OS version 5.2 (or higher).
How do I know what the version number of my TI-Innovator™ Hub App is?
To determine the version of the Hub App that is loaded on your TI-84 Plus CE, follow these steps.
1) Press 2nd [mem]
2) Select option “2: Mem Management/Delete…”
3) Select option “A: Apps”
4) Press the down arrow until the Hub app is selected. Look at the title bar to view the version number of the Hub app.
How do I get the TI-Innovator™ Hub App?
The TI-Innovator™ Hub App is available for download from the TI website at https://education.ti.com/latest.
Can I downgrade my version of the TI-Innovator™ Hub App?
When using the TI-Innovator™ Hub App, you should always use the latest version of the app that is compatible with the TI-84 Plus CE OS on your calculator. Version 5.2 of the TI-Innovator™ Hub App is the latest version and runs on the TI-84 Plus CE OS version 5.2.
With which TI-84 Plus CE OS release will the TI-Innovator™ Hub CE App be pre-loaded?
TI-84 Plus CE calculators that have version 5.2 and later loaded at initial purchase will have the TI-Innovator™ Hub pre-installed. If you have an earlier OS than 5.2, you can update to OS version 5.2 at https://education.ti.com/latest.
Will I need to update the TI-Innovator™ Hub app every time I update the calculator OS?
The TI-Innovator™ Hub app would only need to be updated when new functionality is added to the app. However, it is strongly recommended that you always keep your TI products up to date with the latest OS and versions. When updating your OS always check to see if any apps have updates as well.
Do I need an app to use the TI-Innovator™ Hub with TI-Nspire™ CX technology?
No. Version 4.3 (and higher) of TI-Nspire™ CX technology has all the commands to communicate with the TI-Innovator™ Hub built in.
For more details refer to the TI-Innovator™ System eGuide. To access the eGuide, please click on [View]. If you require further assistance please contact TI-Cares for support at 1-866-846-2844 or E-Mail TI-Cares Customer Support.