Education Technology


Algebra 1: Chirp, Jump, Scatter

by Texas Instruments - Bell Ringer Lesson

Overview

Students will find a best fit line for data graphed as scatter plots.

Key Steps

  • Image

    Students will run a program that contains the data sets for each problem. When they select an option, it will enter the lists of data into L1 and L2. Students are to look at the lists and determine if they can see a trend. 

     

    Students will create a scatter plot and then use the Line command to create a line of best fit.

  • Image

    Then students will use the two points of their line to calculate the equation. Using the equation, students will predict the number of chirps for a given temperature.

  • Image

    Students can compare their line of best fit with the calculator’s linear regression line by adding both lines.