MultiView display View multiple calculations at the same time, compare results and explore patterns on-screen. The MultiView display supports up to four lines.
MathPrint feature See math expressions, symbols and stacked fractions exactly the way they appear in textbooks — no need to adapt to a technical syntax. Also provides quick access to frequently used functions.
Scrolling and editing Easily input data, scroll through entries, make edits and investigate patterns as you would on a graphing calculator.
Toggle key Quickly view fractions, decimals and terms — including Pi — in alternate forms while exploring more advanced topics.
Key Features: Mode menu The menu is structured for easy, intuitive access to commands. Select degrees/radians, floating/fix, Classic/MathPrint or number format.
Memory variables Store real numbers and expressions that result in real numbers as one of seven available memory variables.
Data list editor Enter statistical data in up to three lists, with a maximum of 42 items per list. Any list formulas that are entered can accept all calculator functions. Readily perform one- and two-variable analysis, and display six different regression models.
Solvers Choose from three solvers to use: numeric equation, polynomial and system of linear equations.
Function Table Display a defined function in a tabular form.
Derivative & Integral Determine the numeric derivative and integral for real functions.
Vectors & Matrices Perform vectors and matrices using a vector and matrix entry window — a feature similar to the matrix functionality of TI-84 Plus graphing calculators.
Constants & Conversions Choose from nine physical constants that can be pasted into various windows and an easy-to-use menu that includes 18 Metric/English conversions.
|