Exploring Geometry with Cabri Jr.

Who should attend:
Those who desire to learn more about the features of the TI-84 Plus to assist them in covering topics in geometry.
TI Educational Technology used:
TI-84 Plus or TI-83 Plus
TI-84 Plus Silver Edition or TI-83 Plus Silver Edition
Objectives:
Use technology to explore and investigate modes of teaching geometry.
Experience problem solving situations that take advantage of the exploration/investigation mode of classroom interaction
Work through classroom ready activities that use graphing calculators to enhance students’ understanding and problem solving ability
Develop teachers’ familiarity with the TI-84 Plus and the Cabri Jr. app through hands-on explorations modeling effective classroom use of technology
Course Outline:

The main source of content for this course will be the activities from the Explorations book Cabri Jr.: Interactive Geometry Activities and Investigations. This book will also be offered to participants of the institutes. These activities are classroom ready for teachers to implement right way! Additional activities will be supplemented as determined by the instructor to suit the needs of the participants and the length of the institute. (3, 4 or 5 days)

1.   Betweenness and the Sum of Parts
2.   Angles Formed by Two Intersecting Lines
3.   Angles and Transversals
4.   Perpendicular Bisector Theorem
5.   Shortest Distance Between Points and Lines
6.   Translations in the Plane
7.   Reflections in the Plane
8.   Rotations in the Plane
9.   Connecting Translations, Reflection, and Rotations
10. Dilations in the Plane
11. Proof of the Pythagorean Theorem using Transformations
12. Constructing Triangles
13. Angles of a Triangle
14. Triangle Inequality Theorem
15. Similar Triangles and Proportions
16. Midsegments of a Triangle
17. Ratios in Right Triangles
18. Altitude, Median, and Angle Bisector of a Triangle
19. Centers of a Triangle
20. Properties of the Centers of a Triangle
21. Constructing Quadrilaterals
22. Properties of Quadrilaterals
23. Midsegments of Quadrilaterals
24. Angle Bisectors and Medians of Quadrilaterals
25. Investigating Area Relationships
26. Constructing Circles
27. Angles Formed by Intersecting Chords, Secants, and Tangents
28. Segments Formed by Intersecting Chords, Secants, and Tangents
29. Equations of Circles
Facilities Requirements:
Classroom with chalkboard or white board. Although a computer lab is not needed for this institute, the instructor might want to discuss with the organizer the lab’s availability for TI Connectivity and Internet use.
Materials List:
The Organizer
The following is a list of equipment and materials that the organizer must provide:
High-intensity overhead projector with spare bulbs.
Overhead pens, supply of blank transparency sheets, dry-erase markers for white board if that type of board is used in the classroom, or chalk and erasers for a chalkboard.
Name tags for participants
An LCD projector and screen for use with a laptop computer, TI Presenter and/or TI Smartview.
The instructor may need the organizer to request that participants bring copies of their textbooks so they can plan where technology can best be incorporated into their lesson plans.
The T³ Office
The T³ Office will provide enough copies of:

Cabri™ Jr.: Interactive Geometry Activities and Investigations
Author(s) - Charles Vonder Embse and Eugene Olmstead

The instructor will need to arrange with Texas Instruments Workshop Loan Program
(1-888-917-6411) to provide:

30 TI-84 Plus calculators with the latest version of Cabri Jr.
One TI-84 Plus ViewScreen™ overhead panel with DC power adapter.
Small supply of batteries for the TI-84 Plus calculators.
Supply of TI Connectivity cables.
If desired, TI Presenter.
If desired, TI Navigator.
 
  email to friend     print friendly