Activities for Middle Grades Science with the CBL 2 and the TI-73

This book contains 21 activities for middle-grades science investigations that provide hands-on data collection in the physical, life, and earth/space sciences.
 

Table of Contents

1.   Beverage Tests
2.   Energy from Foods - Part I
3.   Energy from Foods - Part II
4.   Voltage from Dry Cells
5.   Electrolytes Which Liquid Produces the Most Volts?
6.   The Effect of Temperature on the Rate of Dissolving
7.   How Fast was that truck going anyway?
8.   Frictional Forces
9.   How can a clock part measure gravity?
10. Collecting Solar Rays
11. Specific Heat of Metals
12. Wet Sand / Dry Sand
13. Who Says a Watched Pot Never Boils?
14. Beating Hearts
15. Water Quality
16. Probing an Aquatic Ecosystem
17. The Effect of Run-off on Water Turbidity
18. Body Cooling Rate of Animals
19. Sunrise, Sunset Weather Match
20. Treasure Trove
21. Insulating Against the Cold

 
  email to friend     print friendly