Product Name: TI-Navigator™
Model Number/Name: NAV-AP-WW
Product Name: TI-Nspire Navigator™
Model Number/Name: Wireless Cradle
This equipment may be operated in the countries that comprise the member countries of the European Union and the European Free Trade Association. These countries, listed in the following paragraph, are referred to as The European Community throughout this document:
AUSTRIA, DENMARK, FINLAND, FRANCE, GERMANY, ITALY, NETHERLANDS, PORTUGAL, SPAIN, SWEDEN, UNITED KINGDOM, NORWAY, and SWITZERLAND.
The TI-Navigator™ Access Point communicates with either a TI-Navigator™ Network Hub or TI-Nspire™ Navigator™ Wireless Cradle via a wireless 802.11b/g link to provide wireless local area networking (WLAN) capabilities and with a personal computer using a standard USB cable. The TI-Navigator™ Access Point includes one 802.11a and one 802.11b/g radio. In the current model, the 802.11a radio is disabled at the factory and via software preventing it from being configured and used when installed at an end user facility.
Declaration of Conformity
Marking by this symbol:
indicates compliance with the Essential Requirements of the R&TTE Directive of the European Union (1999/5/EC). This equipment meets the following conformance standards:
• Safety: EN 60950-1:2001 + A11:2004
• EMC: EN 55022:2006, EN 55024:1998 + A1:2001 + A2:2003, EN 301-489-1 v1.7.1, EN 301-489-17 v1.3.2, CISPR22:1997, CISPR24; Including: EN 61000-3-2, -3-3, -4-2, -4-3, -4-4, -4-5, -4-6 and -4-11. The product is also licensed as required for additional country specific standards as required for the International Marketplace.
• Radio: EN 300-328 v.1.7.1 (2006-10) Electromagnetic compatibility and Radio spectrum Matters (ERM); Wideband transmission systems; Data transmission equipment operating in the 2,4 GHz ISM band and using wide band modulation techniques. Certifications are harmonized to the EN standards covering essential requirements under article 3.2 of the R&TTE Directive. Compliance includes testing with the supplied integral antenna.
• SAR: EN 50385:2002
European Community Declaration of Conformity
English Hereby, Texas Instruments declares that this TI-Navigator™ Access Point is in compliance with the essential requirements and other relevant provisions of Directive 1999/5/EC. The Declaration of Conformity may be consulted in the Product Stewardship page at education.ti.com.
Dansk Undertegnede Texas Instruments erklærer herved, at følgende udstyr TI-Navigator™ Access Point overholder de væsentlige krav og øvrige relevante krav i direktiv 1999/5/EF. Overensstemmelsesdirektivet (Declaration of Conformity) kan findes på Product Stewardship siden på education.ti.com.
Norsk Texas Instruments erklærer herved at utstyret TI-Navigator™ Access Point er i samsvar med de grunnleggende krav og øvrige relevante krav i direktiv 1999/5/EF. Samsvarserklæringen kan konsulteres på produktforvaltningssiden (Product Stewardship) på education.ti.com.
Suomi Texas Instruments vakuuttaa täten että TI-Navigator™ Access Point tyyppinen laite on direktiivin 1999/5/EY oleellisten vaatimusten ja sitä koskevien direktiivin muiden ehtojen mukainen. Vaatimustenmukaisuusvakuutus on saatavilla tuotteen ympäristövaikutuksen sivulta osoitteessa education.ti.com.
Français Par la présente Texas Instruments déclare que l'appareil TI-Navigator™ Access Point est conforme aux exigences essentielles et aux autres dispositions pertinentes de la directive 1999/5/CE. La déclaration de conformité peut être consultée sur le site education.ti.com à la page Responsabilité Produit (Product Stewardship)
Deutsch Hiermit erklärt Texas Instruments, dass sich das Gerät TI-Navigator™ Access Point in Übereinstimmung mit den grundlegenden Anforderungen und den übrigen einschlägigen Bestimmungen der Richtlinie 1999/5/EG befindet. Die Konformitätserklärung ist unter Produktbetreuung (Product Stewardship) bei education.ti.com einzusehen.
Español Por medio de la presente Texas Instruments declara que el TI-Navigator™ Access Point cumple con los requisitos esenciales y cualesquiera otras disposiciones aplicables o exigibles de la Directiva 1999/5/CE. La Declaración de Conformidad puede consultarse en la página de Administración de Productos (Product Stewardship) en education.ti.com
Italiano Con la presente Texas Instruments dichiara che questo TI-Navigator™ Access Point è conforme ai requisiti essenziali ed alle altre disposizioni pertinenti stabilite dalla direttiva 1999/5/CE. La dichiarazione di conformità può essere consultata sulla pagina Product Stewardship del sito education.ti.com.
Nederlands Hierbij verklaart Texas Instruments dat het toestel TI-Navigator™ Access Point in overeenstemming is met de essentiële eisen en de andere relevante bepalingen van richtlijn 1999/5/EG. De verklaring van overeenstemming kan worden geraadpleegd op de pagina Product Stewardship (Productverantwoordelijkheid) op education.ti.com.
Português Texas Instruments declara que este TI-Navigator™ Access Point está conforme com os requisitos essenciais e outras disposições da Directiva 1999/5/CE. Pode-se consultar a Declaração de Conformidade na página de Gestão de Produto, (Product Stewardship) no sítio education.ti.com.
Svenska Härmed intygar Texas Instruments att denna TTI-Navigator™ Access Point står I överensstämmelse med de väsentliga egenskapskrav och övriga relevanta bestämmelser som framgår av direktiv 1999/5/EG. Förenlighetsdeklarationen kan konsulteras på Produktförvaltningssidan (Product Stewardship) på education.ti.com.
Countries of Operation and Restrictions of Use in the European Community Operation Using the 2.400 to 2.4835 GHz Channels in the European Community
The installer and/or end user should use the configuration utility provided with this product to verify the current channel of operation and to confirm that the device is operating in conformance with the spectrum usage rules for the selected European Community country.
This device is intended to be operated in all countries of the European Community. Additional restrictions of use for the TI-Navigator™ Access Point within the European Community countries in the 2.400 to 2.4835 GHz band are listed below.
• • The frequencies associated with channels 1 to 13 in the 2.400 to 2.4835 GHz band are allowed to be used either indoors or outdoors in all countries of the European Community, except where noted below:
• • In Greece, Italy, Latvia, and Spain the end-user must apply for a license from the national spectrum authority to operate this device outdoors. Please consult the TI Navigator User's Guide for further information regarding restrictions and operating conditions for outdoor configurations.
• • In France, the following operation is permitted:
– Outdoor operation is only permitted using the 2.400 - 2.454 GHz band, which includes channels 1 to 7, at a maximum EIRP of 100 mW (20 dBm).
– Outdoor operation is permitted in the 2.400 to 2.4835 GHz band on channels 1 to 13 at a maximum EIRP of 10 mW (10 dBm).
– Indoor operation is permitted in the 2.400 to 2.4835 GHz band on channels 1 to 13 at a maximum EIRP of 100 mW (20 dBm).
|