TI-Nspire™ TI-Navigator™


Features Summary
The TI-NspireTM NavigatorTM  System is a wireless classroom network that supports teaching and learning activities with TI-Nspire handhelds, further enhancing their effectiveness in the maths and science classroom. This connected approach was developed following research into beneficial types of interactions between teachers and learners, enabling teachers to demonstrate activities, share documents and constructions immediately with the whole class, which supports individual and small group work. The new system is currently being used by pilot schools in England and Scotland to support collaboration, independent learning and assessment of learners’ progress.

Using the TI-Nspire Navigator System, the teacher is able to follow the progress of all learners: individual’s work can be shared with the whole class with or without naming them. Teachers have the opportunity to develop lessons, activities and questions in ways that are enriched by the use of ICT. With revised National Curricula asking teachers to focus on process as well as content, TI-Nspire Navigator adds new teaching options to the already powerful dynamic linking of the TI-Nspire handheld and its document structure.

TI is committed to providing excellent support and professional development in supporting the set-up and implementation of the TI-Nspire Navigator System in your school. If you would like a demonstration of the system or to arrange professional development, please contact us at t3@ti.com. The system will be available to purchase in early 2010.

Features
Class Register
Multiple class management
Seating Chart (which can also include the teacher)
Unique learner username and password
Easy assignment and tracking of documents
Sharing Documents
Status icons identify actions (Collect, Send, Redistribute, Delete, Saved to Portfolio)
Select entire class or group of learners
Easy view of action progress
Portfolio
Personalised Portfolios of collected files
Easy access to .tns files and Quick Poll results directly from the Portfolio window
Class Analysis
Slide Show to demo correct results
Quick class summary result
Save results to Portfolio
Easy view of non-participation
Question Authoring
All authoring done in Question Application in TI-Nspire Teacher Edition Software
Teacher Edition has “send to class” option to share documents through TI-Nspire Navigator
Teacher Edition can import .edc files (Learning Check files)
Easily combine question content with other TI-Nspire applications
Quick Poll
Learners can use text and maths boxes to answer
Results can be saved directly in Portfolio
Poll Details tab to check who has not answered
Screen Capture
Save screens for each learner in their Portfolio
Gallery view of learners’ screens
Make any handheld a live presenter
Auto Refresh option
System Requirements
Minimum Computer Requirements
Operating system: Microsoft® Windows® Vista Ultimate, Vista Business, Vista Home Premium and XP Pro (SP 1, 2 and 3)
Processor: 1.2GHz
Hard disk space: 250MB free
RAM: 1GB (512MB for Windows XP Pro)
Screen resolution: 1024 x 768
CD-ROM drive
Not Supported OS
Microsoft® Windows® Vista Basic and XP Home
Mac OS X
  email to friend     print friendly
COMING SOON