Download Central : Download

To download the following files, click on the file name and save it to a folder on your computer. Record the name of the folder where you saved the file for future reference.

Please note that download times may vary depending on your type of Internet connection - some files are large and may take time to download.
Free Downloads Guidebooks My Collection
 

Explorer Draw App for TI-73 Explorer™ (Concept)


This Calculator Software Application contains two familiar tools, Logo Light and Isometric Dots.

Read the License before continuing. By downloading the application you indicate your agreement with the terms and conditions of the License.

 


Item Name Version Size (KB) Apps Spaces

download Explorer Draw 0.33 38 1

Guidebooks

download Explorer Draw guidebook for TI-73 Explorer (English)   151  

Feature Summary

This Calculator Software Application contains two familiar tools, Logo Light and Isometric Dots. Analyze characteristics and properties of 2-D and 3-D geometric shapes. Draw two-dimensional shapes using the programming commands in Logo Light. Draw representations of three-dimensional cubes using Isometric Dots. Save your images as files or PICs! Make drawings to use in StudyCards™.
Modes Available:
Logo Light contains a minimal set of commands to make drawings and place text on the screen! Use the commands to analyze and draw 2-D shapes. Determine angle measures needed to create regular polygons. Create interesting shapes, patterns and even tessellations using your knowledge of lengths of sides and angles. Place images at chosen coordinates using the AXES and SETPOS commands. Have fun creating PICs to drop into StudyCards!

Isometric Dots mode has an isometric grid to draw 2-D representations of 3-D cube stacks. Build physical models and then draw them on the screen. Save the image as a file to play later or save the image as a PIC to drop into a word processor or make StudyCards. A sample set of cube stacks is also available to test your knowledge. How many cubes do you see?
 

The Explorer Draw App is only available for the TI-73 Explorer Graphing Calculator.

This is a Concept App. Concept Apps have not completed full product testing and/or definition.



Download Instructions