Activity Detail

If you are using a TI-73, TI-83, TI-84 or TI-89, there may be particular math or science applications you will need to download to use certain activities. If you are using TI-Nspire technology, please update your TI-Nspire handheld operating system or computer software to view the latest activities. The latest TI-Nspire operating system was released in June 2009.
Browse by Subject Submit Activity Saved Activities Advanced Search
  


add to saved activities



print this activity
 
Right Triangles are Cool Because of Pythag's Rule
 


Activity Overview

In this activity, students use the Geoboard to determine the length of the sides of a right triangles.

Before the Activity

  • Start the Geoboard App and format it
  • See the attached PDF file for detailed instructions for this activity
  • Print pages 85 - 91 from the attached PDF file for your class


  • During the Activity

    Distribute the page to the class.

    Follow the Activity procedures:
  • Draw a right triangle with leg lengths of 1 unit and draw squares on each side of the triangle


  • Draw right triangles with the different leg lengths given in the table
  • Draw surrounding squares and record areas of the squares
  • Find the relationship between the areas of the squares
  • Understand the Pythagorean Theorem that states - the sum of the square of the length of the legs is equal to the square of the length of the hypotenuse in a right triangle
  • Draw a right angle triangle with sides 3 and 4 and find the length of the hypotenuse
  • Note the length is 5 units


  • Draw four right triangles with length of legs that are different from those used earlier
  • Enter leg lengths, hypotenuse length, leg length squared, and hypotenuse squared in different columns
  • Find the relationship between the leg length squared and the hypotenuse squared
  • Observe that the sum of the leg length squared is equal to the hypotenuse squared and the Pythagorean Theorem is valid in right triangle is A2 + B2 = C2
  • Given the length of the sides of a triangle identify the triangle as acute, right, or obtuse
  • If A2 + B2 > C2 then the triangle is an acute triangle
  • If A2 + B2 = C2 then the triangle is a right triangle
  • If A2 + B2 < C2 then the triangle is an obtuse triangle


    After the Activity

    Review student results:
  • As a class, discuss questions that appeared to be more challenging
  • Re-teach concepts as necessary


    Other Downloads




    view standards alignment
    view textbook alignment

    Subject Area:
    Math : Geometry : Triangles

    Author:
    Texas Instruments

    Level:
    5-8

    Activity Time:
    60 Minutes

    Device:
    TI-73 Explorer™

    Apps:
     

    Software:
     

    Accessories:
     

    Other:
    This is Activity 8 from the EXPLORATIONS Book:
    Shaping Middle Grades Mathematics: Activities for Geoboard and the TI-73



    Report an issue with this activity