Solution 13341: Using the fInt Function Integral Command on the TI-83 Plus Family of Graphing Calculators.
How do I use the fInt Function Integral command on the TI-83 Plus family of graphing calculators?
The fnInt command returns the numerical integral of an expression with regards for real numbers only. The numerical integral is based on the Gauss-Kronrod method. The numerical integral is calculated with respect to the variable, given a lower limit, upper limit and a tolerance. Tolerance is optional and if not specified it is defaulted to 1E-5.
The syntax for the fnInt command is below:
fnInt(expression, variable, lower, upper[,tolerance]), between lower and upper, with specified tolerance.
Example: Find the function integral of A2, for the variable A, with 0 as the lower bound and 1 as the upper bound:
1) Press [MATH] then [9] to select 9:fInt(.
2) Press [ALPHA] [MATH] [x2] [,] [ALPHA] [MATH] [,] [0] [,] [1] [)] [ENTER].
Please see the TI-83 Plus Family guidebooks for additional information.
Last updated: 7/06/2023